public static class FieldEvaluator.ValuesOutsideTableInterpolationEnum extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CONSTANT
Returns the boundary value as interpolation result
|
static int |
_CUBIC
Extrapolates from the boundary out into space using the cubic extrapolation method
|
static int |
_EXTRAPOLATE
Extrapolates from the boundary out into space using the same interpolation method that the interpolator for interior table values uses
|
static int |
_LINEAR
Extrapolates from the boundary out into space using the linear extrapolation method
|
static int |
_PARABOLIC
Extrapolates from the boundary out into space using the parabolic extrapolation method
|
static int |
_UNDEFINED
No interpolation result
|
static FieldEvaluator.ValuesOutsideTableInterpolationEnum |
CONSTANT
Returns the boundary value as interpolation result
|
static FieldEvaluator.ValuesOutsideTableInterpolationEnum |
CUBIC
Extrapolates from the boundary out into space using the cubic extrapolation method
|
static FieldEvaluator.ValuesOutsideTableInterpolationEnum |
EXTRAPOLATE
Extrapolates from the boundary out into space using the same interpolation method that the interpolator for interior table values uses
|
static FieldEvaluator.ValuesOutsideTableInterpolationEnum |
LINEAR
Extrapolates from the boundary out into space using the linear extrapolation method
|
static FieldEvaluator.ValuesOutsideTableInterpolationEnum |
PARABOLIC
Extrapolates from the boundary out into space using the parabolic extrapolation method
|
static FieldEvaluator.ValuesOutsideTableInterpolationEnum |
UNDEFINED
No interpolation result
|
Modifier and Type | Method and Description |
---|---|
static FieldEvaluator.ValuesOutsideTableInterpolationEnum |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FieldEvaluator.ValuesOutsideTableInterpolationEnum |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FieldEvaluator.ValuesOutsideTableInterpolationEnum[] |
values()
Returns an array that contains the values for this enum.
|
public static final FieldEvaluator.ValuesOutsideTableInterpolationEnum UNDEFINED
public static final FieldEvaluator.ValuesOutsideTableInterpolationEnum EXTRAPOLATE
public static final FieldEvaluator.ValuesOutsideTableInterpolationEnum CONSTANT
public static final FieldEvaluator.ValuesOutsideTableInterpolationEnum LINEAR
public static final FieldEvaluator.ValuesOutsideTableInterpolationEnum PARABOLIC
public static final FieldEvaluator.ValuesOutsideTableInterpolationEnum CUBIC
public static final int _UNDEFINED
public static final int _EXTRAPOLATE
public static final int _CONSTANT
public static final int _LINEAR
public static final int _PARABOLIC
public static final int _CUBIC
public static FieldEvaluator.ValuesOutsideTableInterpolationEnum valueOf(int value)
public static FieldEvaluator.ValuesOutsideTableInterpolationEnum valueOf(String name)
public static FieldEvaluator.ValuesOutsideTableInterpolationEnum[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.