Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for Vehicle Design.
|
Modifier and Type | Field and Description |
---|---|
static MirrorCertificationBuilder.EyePointMethodType |
MirrorCertificationBuilder.EyePointMethodType.BY_ECE_VISION_POINTS_FEATURE
Represents using ECE Vision Point feature to get eye point
|
static MirrorCertificationBuilder.EyePointMethodType |
MirrorCertificationBuilder.EyePointMethodType.BY_HIP_POINT
Represents using Hip Point to calculate the eye point
|
Modifier and Type | Method and Description |
---|---|
MirrorCertificationBuilder.EyePointMethodType |
MirrorCertificationBuilder.eyePointMethod()
Returns the method to define the eye point.
|
static MirrorCertificationBuilder.EyePointMethodType |
MirrorCertificationBuilder.EyePointMethodType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MirrorCertificationBuilder.EyePointMethodType |
MirrorCertificationBuilder.EyePointMethodType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MirrorCertificationBuilder.EyePointMethodType[] |
MirrorCertificationBuilder.EyePointMethodType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MirrorCertificationBuilder.setEyePointMethod(MirrorCertificationBuilder.EyePointMethodType eyePointMethod)
License requirements: nx_general_packaging ("NX General Packaging") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.