public static class MirrorCertificationBuilder.EyePointMethodType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BY_ECE_VISION_POINTS_FEATURE
Represents using ECE Vision Point feature to get eye point
|
static int |
_BY_HIP_POINT
Represents using Hip Point to calculate the eye point
|
static MirrorCertificationBuilder.EyePointMethodType |
BY_ECE_VISION_POINTS_FEATURE
Represents using ECE Vision Point feature to get eye point
|
static MirrorCertificationBuilder.EyePointMethodType |
BY_HIP_POINT
Represents using Hip Point to calculate the eye point
|
Modifier and Type | Method and Description |
---|---|
static MirrorCertificationBuilder.EyePointMethodType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MirrorCertificationBuilder.EyePointMethodType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MirrorCertificationBuilder.EyePointMethodType[] |
values()
Returns an array that contains the values for this enum.
|
public static final MirrorCertificationBuilder.EyePointMethodType BY_ECE_VISION_POINTS_FEATURE
public static final MirrorCertificationBuilder.EyePointMethodType BY_HIP_POINT
public static final int _BY_ECE_VISION_POINTS_FEATURE
public static final int _BY_HIP_POINT
public static MirrorCertificationBuilder.EyePointMethodType valueOf(int value)
public static MirrorCertificationBuilder.EyePointMethodType valueOf(String name)
public static MirrorCertificationBuilder.EyePointMethodType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.