Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for Vehicle Design.
|
Modifier and Type | Field and Description |
---|---|
static MirrorCertificationBuilder.EyeFromOptionType |
MirrorCertificationBuilder.EyeFromOptionType.OTHER_COMPONENT
Represents eyellipse feature is from the other component Part
|
static MirrorCertificationBuilder.EyeFromOptionType |
MirrorCertificationBuilder.EyeFromOptionType.ROOT_PART
Represents eyellipse feature is from root part
|
static MirrorCertificationBuilder.EyeFromOptionType |
MirrorCertificationBuilder.EyeFromOptionType.WORK_PART
Represents eyellipse feature is from work part
|
Modifier and Type | Method and Description |
---|---|
MirrorCertificationBuilder.EyeFromOptionType |
MirrorCertificationBuilder.useEyeFrom()
Returns the part that the eye is from.
|
static MirrorCertificationBuilder.EyeFromOptionType |
MirrorCertificationBuilder.EyeFromOptionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MirrorCertificationBuilder.EyeFromOptionType |
MirrorCertificationBuilder.EyeFromOptionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MirrorCertificationBuilder.EyeFromOptionType[] |
MirrorCertificationBuilder.EyeFromOptionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MirrorCertificationBuilder.setUseEyeFrom(MirrorCertificationBuilder.EyeFromOptionType useEyeFrom)
License requirements: nx_general_packaging ("NX General Packaging") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.