public static class MirrorCertificationBuilder.EyeFromOptionType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_OTHER_COMPONENT
Represents eyellipse feature is from the other component Part
|
static int |
_ROOT_PART
Represents eyellipse feature is from root part
|
static int |
_WORK_PART
Represents eyellipse feature is from work part
|
static MirrorCertificationBuilder.EyeFromOptionType |
OTHER_COMPONENT
Represents eyellipse feature is from the other component Part
|
static MirrorCertificationBuilder.EyeFromOptionType |
ROOT_PART
Represents eyellipse feature is from root part
|
static MirrorCertificationBuilder.EyeFromOptionType |
WORK_PART
Represents eyellipse feature is from work part
|
Modifier and Type | Method and Description |
---|---|
static MirrorCertificationBuilder.EyeFromOptionType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MirrorCertificationBuilder.EyeFromOptionType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MirrorCertificationBuilder.EyeFromOptionType[] |
values()
Returns an array that contains the values for this enum.
|
public static final MirrorCertificationBuilder.EyeFromOptionType WORK_PART
public static final MirrorCertificationBuilder.EyeFromOptionType ROOT_PART
public static final MirrorCertificationBuilder.EyeFromOptionType OTHER_COMPONENT
public static final int _WORK_PART
public static final int _ROOT_PART
public static final int _OTHER_COMPONENT
public static MirrorCertificationBuilder.EyeFromOptionType valueOf(int value)
public static MirrorCertificationBuilder.EyeFromOptionType valueOf(String name)
public static MirrorCertificationBuilder.EyeFromOptionType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.