Package | Description |
---|---|
nxopen.features.subdivision |
Provides classes and interfaces for Subdivision Body feature.
|
Modifier and Type | Field and Description |
---|---|
static SubdivisionExtrudeCageBuilder.ScalingMethodType |
SubdivisionExtrudeCageBuilder.ScalingMethodType.LINEAR
Scale in the specified direction
|
static SubdivisionExtrudeCageBuilder.ScalingMethodType |
SubdivisionExtrudeCageBuilder.ScalingMethodType.PLANAR
Scale in the plane normal to specified direction
|
static SubdivisionExtrudeCageBuilder.ScalingMethodType |
SubdivisionExtrudeCageBuilder.ScalingMethodType.UNIFORM
Scale uniformly all the directions
|
Modifier and Type | Method and Description |
---|---|
SubdivisionExtrudeCageBuilder.ScalingMethodType |
SubdivisionExtrudeCageBuilder.scalingMethod()
Returns the scaling method.
|
static SubdivisionExtrudeCageBuilder.ScalingMethodType |
SubdivisionExtrudeCageBuilder.ScalingMethodType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SubdivisionExtrudeCageBuilder.ScalingMethodType |
SubdivisionExtrudeCageBuilder.ScalingMethodType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SubdivisionExtrudeCageBuilder.ScalingMethodType[] |
SubdivisionExtrudeCageBuilder.ScalingMethodType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SubdivisionExtrudeCageBuilder.setScalingMethod(SubdivisionExtrudeCageBuilder.ScalingMethodType scalingMethod)
License requirements: nx_subdivision (" NX SUBDIVISION") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.