public static class SubdivisionExtrudeCageBuilder.ScalingMethodType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_LINEAR
Scale in the specified direction
|
static int |
_PLANAR
Scale in the plane normal to specified direction
|
static int |
_UNIFORM
Scale uniformly all the directions
|
static SubdivisionExtrudeCageBuilder.ScalingMethodType |
LINEAR
Scale in the specified direction
|
static SubdivisionExtrudeCageBuilder.ScalingMethodType |
PLANAR
Scale in the plane normal to specified direction
|
static SubdivisionExtrudeCageBuilder.ScalingMethodType |
UNIFORM
Scale uniformly all the directions
|
Modifier and Type | Method and Description |
---|---|
static SubdivisionExtrudeCageBuilder.ScalingMethodType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SubdivisionExtrudeCageBuilder.ScalingMethodType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SubdivisionExtrudeCageBuilder.ScalingMethodType[] |
values()
Returns an array that contains the values for this enum.
|
public static final SubdivisionExtrudeCageBuilder.ScalingMethodType LINEAR
public static final SubdivisionExtrudeCageBuilder.ScalingMethodType PLANAR
public static final SubdivisionExtrudeCageBuilder.ScalingMethodType UNIFORM
public static final int _LINEAR
public static final int _PLANAR
public static final int _UNIFORM
public static SubdivisionExtrudeCageBuilder.ScalingMethodType valueOf(int value)
public static SubdivisionExtrudeCageBuilder.ScalingMethodType valueOf(String name)
public static SubdivisionExtrudeCageBuilder.ScalingMethodType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.