Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static StiffenerBuilder.EdgeReinforcementAlignmentMethod |
StiffenerBuilder.EdgeReinforcementAlignmentMethod.CENTER
Center the Edge Reinforcement on the selected edge
|
static StiffenerBuilder.EdgeReinforcementAlignmentMethod |
StiffenerBuilder.EdgeReinforcementAlignmentMethod.GUIDE_EDGE
Place the end of the Edge Reinforcement on the selected edge
|
static StiffenerBuilder.EdgeReinforcementAlignmentMethod |
StiffenerBuilder.EdgeReinforcementAlignmentMethod.OPPOSITE_GUIDE
Place the end of the Edge Reinforcement on the edge opposite the selected edge
|
Modifier and Type | Method and Description |
---|---|
StiffenerBuilder.EdgeReinforcementAlignmentMethod |
StiffenerBuilder.edgeReinforcementAlignment()
Returns the edge reinforcement alignment
License requirements: None. |
static StiffenerBuilder.EdgeReinforcementAlignmentMethod |
StiffenerBuilder.EdgeReinforcementAlignmentMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StiffenerBuilder.EdgeReinforcementAlignmentMethod |
StiffenerBuilder.EdgeReinforcementAlignmentMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StiffenerBuilder.EdgeReinforcementAlignmentMethod[] |
StiffenerBuilder.EdgeReinforcementAlignmentMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StiffenerBuilder.setEdgeReinforcementAlignment(StiffenerBuilder.EdgeReinforcementAlignmentMethod edgeReinforcementAlignment)
License requirements: nx_ship_detail ("Ship Detail Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.