public static class StiffenerBuilder.EdgeReinforcementAlignmentMethod extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CENTER
Center the Edge Reinforcement on the selected edge
|
static int |
_GUIDE_EDGE
Place the end of the Edge Reinforcement on the selected edge
|
static int |
_OPPOSITE_GUIDE
Place the end of the Edge Reinforcement on the edge opposite the selected edge
|
static StiffenerBuilder.EdgeReinforcementAlignmentMethod |
CENTER
Center the Edge Reinforcement on the selected edge
|
static StiffenerBuilder.EdgeReinforcementAlignmentMethod |
GUIDE_EDGE
Place the end of the Edge Reinforcement on the selected edge
|
static StiffenerBuilder.EdgeReinforcementAlignmentMethod |
OPPOSITE_GUIDE
Place the end of the Edge Reinforcement on the edge opposite the selected edge
|
Modifier and Type | Method and Description |
---|---|
static StiffenerBuilder.EdgeReinforcementAlignmentMethod |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StiffenerBuilder.EdgeReinforcementAlignmentMethod |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StiffenerBuilder.EdgeReinforcementAlignmentMethod[] |
values()
Returns an array that contains the values for this enum.
|
public static final StiffenerBuilder.EdgeReinforcementAlignmentMethod CENTER
public static final StiffenerBuilder.EdgeReinforcementAlignmentMethod GUIDE_EDGE
public static final StiffenerBuilder.EdgeReinforcementAlignmentMethod OPPOSITE_GUIDE
public static final int _CENTER
public static final int _GUIDE_EDGE
public static final int _OPPOSITE_GUIDE
public static StiffenerBuilder.EdgeReinforcementAlignmentMethod valueOf(int value)
public static StiffenerBuilder.EdgeReinforcementAlignmentMethod valueOf(String name)
public static StiffenerBuilder.EdgeReinforcementAlignmentMethod[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.