Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static ShipnameFieldBuilderType |
ShipnameFieldBuilderType.ANY
Field whose value will be a user enterred string
|
static ShipnameFieldBuilderType |
ShipnameFieldBuilderType.CONTEXT_ATTRIBUTE_MAP
Field whose value comes from context attribute
|
static ShipnameFieldBuilderType |
ShipnameFieldBuilderType.FIXED
Field with an unchanging string
|
static ShipnameFieldBuilderType |
ShipnameFieldBuilderType.INDEX
Field which will have a number generated
|
static ShipnameFieldBuilderType |
ShipnameFieldBuilderType.NONE
Unknown Field Type
|
static ShipnameFieldBuilderType |
ShipnameFieldBuilderType.OPTION
Field whose value can be one of several strings
|
static ShipnameFieldBuilderType |
ShipnameFieldBuilderType.POSITION_INFORMATION
Field which is generated from mold face plane indicate part location
|
static ShipnameFieldBuilderType |
ShipnameFieldBuilderType.SECTION_INFORMATION
Field whose value comes from section
|
Modifier and Type | Method and Description |
---|---|
static ShipnameFieldBuilderType |
ShipnameFieldBuilderType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ShipnameFieldBuilderType |
ShipnameFieldBuilderType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ShipnameFieldBuilderType[] |
ShipnameFieldBuilderType.values()
Returns an array that contains the values for this enum.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.