public class ShipnameFieldBuilderType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ANY
Field whose value will be a user enterred string
|
static int |
_CONTEXT_ATTRIBUTE_MAP
Field whose value comes from context attribute
|
static int |
_FIXED
Field with an unchanging string
|
static int |
_INDEX
Field which will have a number generated
|
static int |
_NONE
Unknown Field Type
|
static int |
_OPTION
Field whose value can be one of several strings
|
static int |
_POSITION_INFORMATION
Field which is generated from mold face plane indicate part location
|
static int |
_SECTION_INFORMATION
Field whose value comes from section
|
static ShipnameFieldBuilderType |
ANY
Field whose value will be a user enterred string
|
static ShipnameFieldBuilderType |
CONTEXT_ATTRIBUTE_MAP
Field whose value comes from context attribute
|
static ShipnameFieldBuilderType |
FIXED
Field with an unchanging string
|
static ShipnameFieldBuilderType |
INDEX
Field which will have a number generated
|
static ShipnameFieldBuilderType |
NONE
Unknown Field Type
|
static ShipnameFieldBuilderType |
OPTION
Field whose value can be one of several strings
|
static ShipnameFieldBuilderType |
POSITION_INFORMATION
Field which is generated from mold face plane indicate part location
|
static ShipnameFieldBuilderType |
SECTION_INFORMATION
Field whose value comes from section
|
Modifier and Type | Method and Description |
---|---|
static ShipnameFieldBuilderType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ShipnameFieldBuilderType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ShipnameFieldBuilderType[] |
values()
Returns an array that contains the values for this enum.
|
public static final ShipnameFieldBuilderType FIXED
public static final ShipnameFieldBuilderType OPTION
public static final ShipnameFieldBuilderType INDEX
public static final ShipnameFieldBuilderType ANY
public static final ShipnameFieldBuilderType POSITION_INFORMATION
public static final ShipnameFieldBuilderType CONTEXT_ATTRIBUTE_MAP
public static final ShipnameFieldBuilderType SECTION_INFORMATION
public static final ShipnameFieldBuilderType NONE
public static final int _FIXED
public static final int _OPTION
public static final int _INDEX
public static final int _ANY
public static final int _POSITION_INFORMATION
public static final int _CONTEXT_ATTRIBUTE_MAP
public static final int _SECTION_INFORMATION
public static final int _NONE
public static ShipnameFieldBuilderType valueOf(int value)
public static ShipnameFieldBuilderType valueOf(String name)
public static ShipnameFieldBuilderType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.