Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static ShellTemplateBuilder.SightLineCutTypes |
ShellTemplateBuilder.SightLineCutTypes.NONE
Do not add sight line cuts.
|
static ShellTemplateBuilder.SightLineCutTypes |
ShellTemplateBuilder.SightLineCutTypes.TOWARD_END
Add sight line cuts from the sight line toward the end side of each template.
|
static ShellTemplateBuilder.SightLineCutTypes |
ShellTemplateBuilder.SightLineCutTypes.TOWARD_START
Add sight line cuts from sight line toward the start side of each template.
|
Modifier and Type | Method and Description |
---|---|
ShellTemplateBuilder.SightLineCutTypes |
ShellTemplateBuilder.sightLineCutType()
Returns the value that specifies if and where to create sight line cuts
License requirements: None. |
static ShellTemplateBuilder.SightLineCutTypes |
ShellTemplateBuilder.SightLineCutTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ShellTemplateBuilder.SightLineCutTypes |
ShellTemplateBuilder.SightLineCutTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ShellTemplateBuilder.SightLineCutTypes[] |
ShellTemplateBuilder.SightLineCutTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ShellTemplateBuilder.setSightLineCutType(ShellTemplateBuilder.SightLineCutTypes sightLineCutType)
License requirements: nx_ship_concept ("Ship Concept") OR nx_ship_mfg_prep ("Ship Manufacturing") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.