public static class ShellTemplateBuilder.SightLineCutTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NONE
Do not add sight line cuts.
|
static int |
_TOWARD_END
Add sight line cuts from the sight line toward the end side of each template.
|
static int |
_TOWARD_START
Add sight line cuts from sight line toward the start side of each template.
|
static ShellTemplateBuilder.SightLineCutTypes |
NONE
Do not add sight line cuts.
|
static ShellTemplateBuilder.SightLineCutTypes |
TOWARD_END
Add sight line cuts from the sight line toward the end side of each template.
|
static ShellTemplateBuilder.SightLineCutTypes |
TOWARD_START
Add sight line cuts from sight line toward the start side of each template.
|
Modifier and Type | Method and Description |
---|---|
static ShellTemplateBuilder.SightLineCutTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ShellTemplateBuilder.SightLineCutTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ShellTemplateBuilder.SightLineCutTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final ShellTemplateBuilder.SightLineCutTypes NONE
public static final ShellTemplateBuilder.SightLineCutTypes TOWARD_START
public static final ShellTemplateBuilder.SightLineCutTypes TOWARD_END
public static final int _NONE
public static final int _TOWARD_START
public static final int _TOWARD_END
public static ShellTemplateBuilder.SightLineCutTypes valueOf(int value)
public static ShellTemplateBuilder.SightLineCutTypes valueOf(String name)
public static ShellTemplateBuilder.SightLineCutTypes[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.