Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static ShellTemplateBuilder.CornerCutTypes |
ShellTemplateBuilder.CornerCutTypes.END
Add corner cuts on the end side of each template.
|
static ShellTemplateBuilder.CornerCutTypes |
ShellTemplateBuilder.CornerCutTypes.NONE
Do not add corner cuts.
|
static ShellTemplateBuilder.CornerCutTypes |
ShellTemplateBuilder.CornerCutTypes.START
Add corner cuts on the start side of each template.
|
Modifier and Type | Method and Description |
---|---|
ShellTemplateBuilder.CornerCutTypes |
ShellTemplateBuilder.cornerCutType()
Returns the value that specifies if and where to create corner cuts
License requirements: None. |
static ShellTemplateBuilder.CornerCutTypes |
ShellTemplateBuilder.CornerCutTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ShellTemplateBuilder.CornerCutTypes |
ShellTemplateBuilder.CornerCutTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ShellTemplateBuilder.CornerCutTypes[] |
ShellTemplateBuilder.CornerCutTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ShellTemplateBuilder.setCornerCutType(ShellTemplateBuilder.CornerCutTypes cornerCutType)
License requirements: nx_ship_concept ("Ship Concept") OR nx_ship_mfg_prep ("Ship Manufacturing") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.