public static class ShellTemplateBuilder.CornerCutTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_END
Add corner cuts on the end side of each template.
|
static int |
_NONE
Do not add corner cuts.
|
static int |
_START
Add corner cuts on the start side of each template.
|
static ShellTemplateBuilder.CornerCutTypes |
END
Add corner cuts on the end side of each template.
|
static ShellTemplateBuilder.CornerCutTypes |
NONE
Do not add corner cuts.
|
static ShellTemplateBuilder.CornerCutTypes |
START
Add corner cuts on the start side of each template.
|
Modifier and Type | Method and Description |
---|---|
static ShellTemplateBuilder.CornerCutTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ShellTemplateBuilder.CornerCutTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ShellTemplateBuilder.CornerCutTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final ShellTemplateBuilder.CornerCutTypes NONE
public static final ShellTemplateBuilder.CornerCutTypes START
public static final ShellTemplateBuilder.CornerCutTypes END
public static final int _NONE
public static final int _START
public static final int _END
public static ShellTemplateBuilder.CornerCutTypes valueOf(int value)
public static ShellTemplateBuilder.CornerCutTypes valueOf(String name)
public static ShellTemplateBuilder.CornerCutTypes[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.