Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static PlateBoundaryOptionBuilder.SplitKnuckleTypes |
PlateBoundaryOptionBuilder.SplitKnuckleTypes.MITERED
Two plates which are split and mitered and whoes side faces at knuckle edge are touching.
|
static PlateBoundaryOptionBuilder.SplitKnuckleTypes |
PlateBoundaryOptionBuilder.SplitKnuckleTypes.SQUARE_CUT
The plate side faces at knuckle edge are normal to the molding face.
|
Modifier and Type | Method and Description |
---|---|
static PlateBoundaryOptionBuilder.SplitKnuckleTypes |
PlateBoundaryOptionBuilder.SplitKnuckleTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PlateBoundaryOptionBuilder.SplitKnuckleTypes |
PlateBoundaryOptionBuilder.SplitKnuckleTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PlateBoundaryOptionBuilder.SplitKnuckleTypes[] |
PlateBoundaryOptionBuilder.SplitKnuckleTypes.values()
Returns an array that contains the values for this enum.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.