public static class PlateBoundaryOptionBuilder.SplitKnuckleTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_MITERED
Two plates which are split and mitered and whoes side faces at knuckle edge are touching.
|
static int |
_SQUARE_CUT
The plate side faces at knuckle edge are normal to the molding face.
|
static PlateBoundaryOptionBuilder.SplitKnuckleTypes |
MITERED
Two plates which are split and mitered and whoes side faces at knuckle edge are touching.
|
static PlateBoundaryOptionBuilder.SplitKnuckleTypes |
SQUARE_CUT
The plate side faces at knuckle edge are normal to the molding face.
|
Modifier and Type | Method and Description |
---|---|
static PlateBoundaryOptionBuilder.SplitKnuckleTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PlateBoundaryOptionBuilder.SplitKnuckleTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PlateBoundaryOptionBuilder.SplitKnuckleTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final PlateBoundaryOptionBuilder.SplitKnuckleTypes MITERED
public static final PlateBoundaryOptionBuilder.SplitKnuckleTypes SQUARE_CUT
public static final int _MITERED
public static final int _SQUARE_CUT
public static PlateBoundaryOptionBuilder.SplitKnuckleTypes valueOf(int value)
public static PlateBoundaryOptionBuilder.SplitKnuckleTypes valueOf(String name)
public static PlateBoundaryOptionBuilder.SplitKnuckleTypes[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.