Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static PenetrationRequest.CompensationType |
PenetrationRequest.CompensationType.DOUBLE_SLEEVE |
static PenetrationRequest.CompensationType |
PenetrationRequest.CompensationType.FLANGE |
static PenetrationRequest.CompensationType |
PenetrationRequest.CompensationType.NON_STANDARD |
static PenetrationRequest.CompensationType |
PenetrationRequest.CompensationType.NOT_REQUIRED |
static PenetrationRequest.CompensationType |
PenetrationRequest.CompensationType.SLEEVE |
static PenetrationRequest.CompensationType |
PenetrationRequest.CompensationType.STANDARD |
Modifier and Type | Method and Description |
---|---|
PenetrationRequest.CompensationType |
PenetrationRequestBuilder.compensationType()
Returns the compensation type
License requirements: None. |
static PenetrationRequest.CompensationType |
PenetrationRequest.CompensationType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PenetrationRequest.CompensationType |
PenetrationRequest.CompensationType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PenetrationRequest.CompensationType[] |
PenetrationRequest.CompensationType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PenetrationRequestBuilder.setCompensationType(PenetrationRequest.CompensationType enumCompensationType)
License requirements: nx_penetration_mgmt ("Penetration Management") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.