public static class PenetrationRequest.CompensationType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DOUBLE_SLEEVE |
static int |
_FLANGE |
static int |
_NON_STANDARD |
static int |
_NOT_REQUIRED |
static int |
_SLEEVE |
static int |
_STANDARD |
static PenetrationRequest.CompensationType |
DOUBLE_SLEEVE |
static PenetrationRequest.CompensationType |
FLANGE |
static PenetrationRequest.CompensationType |
NON_STANDARD |
static PenetrationRequest.CompensationType |
NOT_REQUIRED |
static PenetrationRequest.CompensationType |
SLEEVE |
static PenetrationRequest.CompensationType |
STANDARD |
Modifier and Type | Method and Description |
---|---|
static PenetrationRequest.CompensationType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PenetrationRequest.CompensationType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PenetrationRequest.CompensationType[] |
values()
Returns an array that contains the values for this enum.
|
public static final PenetrationRequest.CompensationType NOT_REQUIRED
public static final PenetrationRequest.CompensationType STANDARD
public static final PenetrationRequest.CompensationType NON_STANDARD
public static final PenetrationRequest.CompensationType SLEEVE
public static final PenetrationRequest.CompensationType DOUBLE_SLEEVE
public static final PenetrationRequest.CompensationType FLANGE
public static final int _NOT_REQUIRED
public static final int _STANDARD
public static final int _NON_STANDARD
public static final int _SLEEVE
public static final int _DOUBLE_SLEEVE
public static final int _FLANGE
public static PenetrationRequest.CompensationType valueOf(int value)
public static PenetrationRequest.CompensationType valueOf(String name)
public static PenetrationRequest.CompensationType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.