Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static OrientationPointMethodsBuilder.MeasureAlongTypes |
OrientationPointMethodsBuilder.MeasureAlongTypes.AXIS
The distance is measured along the orthogonal direction closest to the landing curve tangent direction.
|
static OrientationPointMethodsBuilder.MeasureAlongTypes |
OrientationPointMethodsBuilder.MeasureAlongTypes.CURVE
The distance is measured along the landing curve.
|
Modifier and Type | Method and Description |
---|---|
OrientationPointMethodsBuilder.MeasureAlongTypes |
OrientationPointMethodsBuilder.measureAlong()
Returns the indication of how to measure the distance used to determine the boundary of the region.
|
static OrientationPointMethodsBuilder.MeasureAlongTypes |
OrientationPointMethodsBuilder.MeasureAlongTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OrientationPointMethodsBuilder.MeasureAlongTypes |
OrientationPointMethodsBuilder.MeasureAlongTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OrientationPointMethodsBuilder.MeasureAlongTypes[] |
OrientationPointMethodsBuilder.MeasureAlongTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
OrientationPointMethodsBuilder.setMeasureAlong(OrientationPointMethodsBuilder.MeasureAlongTypes measureAlong)
License requirements: nx_ship_basic ("Ship Basic Design") OR nx_ship_detail ("Ship Detail Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.