public static class OrientationPointMethodsBuilder.MeasureAlongTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_AXIS
The distance is measured along the orthogonal direction closest to the landing curve tangent direction.
|
static int |
_CURVE
The distance is measured along the landing curve.
|
static OrientationPointMethodsBuilder.MeasureAlongTypes |
AXIS
The distance is measured along the orthogonal direction closest to the landing curve tangent direction.
|
static OrientationPointMethodsBuilder.MeasureAlongTypes |
CURVE
The distance is measured along the landing curve.
|
Modifier and Type | Method and Description |
---|---|
static OrientationPointMethodsBuilder.MeasureAlongTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OrientationPointMethodsBuilder.MeasureAlongTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OrientationPointMethodsBuilder.MeasureAlongTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final OrientationPointMethodsBuilder.MeasureAlongTypes CURVE
public static final OrientationPointMethodsBuilder.MeasureAlongTypes AXIS
public static final int _CURVE
public static final int _AXIS
public static OrientationPointMethodsBuilder.MeasureAlongTypes valueOf(int value)
public static OrientationPointMethodsBuilder.MeasureAlongTypes valueOf(String name)
public static OrientationPointMethodsBuilder.MeasureAlongTypes[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.