Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static MirrorShipStructureBuilder.Types |
MirrorShipStructureBuilder.Types.FEATURE
The feature type which is valid only in ship basic design application.
|
static MirrorShipStructureBuilder.Types |
MirrorShipStructureBuilder.Types.STRUCTURE_SYSTEM
The structure system type.
|
Modifier and Type | Method and Description |
---|---|
MirrorShipStructureBuilder.Types |
MirrorShipStructureBuilder.selectionType()
Returns the selection type, which is structure system or feature.
|
static MirrorShipStructureBuilder.Types |
MirrorShipStructureBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MirrorShipStructureBuilder.Types |
MirrorShipStructureBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MirrorShipStructureBuilder.Types[] |
MirrorShipStructureBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MirrorShipStructureBuilder.setSelectionType(MirrorShipStructureBuilder.Types type)
License requirements: nx_ship_detail ("Ship Detail Design") OR nx_ship_basic ("Ship Basic Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.