public static class MirrorShipStructureBuilder.Types extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FEATURE
The feature type which is valid only in ship basic design application.
|
static int |
_STRUCTURE_SYSTEM
The structure system type.
|
static MirrorShipStructureBuilder.Types |
FEATURE
The feature type which is valid only in ship basic design application.
|
static MirrorShipStructureBuilder.Types |
STRUCTURE_SYSTEM
The structure system type.
|
Modifier and Type | Method and Description |
---|---|
static MirrorShipStructureBuilder.Types |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MirrorShipStructureBuilder.Types |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MirrorShipStructureBuilder.Types[] |
values()
Returns an array that contains the values for this enum.
|
public static final MirrorShipStructureBuilder.Types STRUCTURE_SYSTEM
public static final MirrorShipStructureBuilder.Types FEATURE
public static final int _STRUCTURE_SYSTEM
public static final int _FEATURE
public static MirrorShipStructureBuilder.Types valueOf(int value)
public static MirrorShipStructureBuilder.Types valueOf(String name)
public static MirrorShipStructureBuilder.Types[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.