Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static MirrorShipStructureBuilder.MirrorApproach |
MirrorShipStructureBuilder.MirrorApproach.COPY_SOURCE_FEATURES_AND_REPARENT
The approach by copy source features and reparenting.
|
static MirrorShipStructureBuilder.MirrorApproach |
MirrorShipStructureBuilder.MirrorApproach.CREATE_LINKED_MIRROR_BODY
The approach by creating linked mirror body.
|
Modifier and Type | Method and Description |
---|---|
MirrorShipStructureBuilder.MirrorApproach |
MirrorShipStructureBuilder.mirrorApproachOption()
Returns an option to determines the approach to copy and mirror ship standard parts.
|
static MirrorShipStructureBuilder.MirrorApproach |
MirrorShipStructureBuilder.MirrorApproach.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MirrorShipStructureBuilder.MirrorApproach |
MirrorShipStructureBuilder.MirrorApproach.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MirrorShipStructureBuilder.MirrorApproach[] |
MirrorShipStructureBuilder.MirrorApproach.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MirrorShipStructureBuilder.setMirrorApproachOption(MirrorShipStructureBuilder.MirrorApproach mirrorApproachOption)
License requirements: nx_ship_detail ("Ship Detail Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.