public static class MirrorShipStructureBuilder.MirrorApproach extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_COPY_SOURCE_FEATURES_AND_REPARENT
The approach by copy source features and reparenting.
|
static int |
_CREATE_LINKED_MIRROR_BODY
The approach by creating linked mirror body.
|
static MirrorShipStructureBuilder.MirrorApproach |
COPY_SOURCE_FEATURES_AND_REPARENT
The approach by copy source features and reparenting.
|
static MirrorShipStructureBuilder.MirrorApproach |
CREATE_LINKED_MIRROR_BODY
The approach by creating linked mirror body.
|
Modifier and Type | Method and Description |
---|---|
static MirrorShipStructureBuilder.MirrorApproach |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MirrorShipStructureBuilder.MirrorApproach |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MirrorShipStructureBuilder.MirrorApproach[] |
values()
Returns an array that contains the values for this enum.
|
public static final MirrorShipStructureBuilder.MirrorApproach CREATE_LINKED_MIRROR_BODY
public static final MirrorShipStructureBuilder.MirrorApproach COPY_SOURCE_FEATURES_AND_REPARENT
public static final int _CREATE_LINKED_MIRROR_BODY
public static final int _COPY_SOURCE_FEATURES_AND_REPARENT
public static MirrorShipStructureBuilder.MirrorApproach valueOf(int value)
public static MirrorShipStructureBuilder.MirrorApproach valueOf(String name)
public static MirrorShipStructureBuilder.MirrorApproach[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.