Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Interface and Description |
---|---|
interface |
DeckBuilder
This class is used to create or edit a
Deck feature. |
interface |
EdgeReinforcementBuilder
Represents a
EdgeReinforcement builder which is used to create or edit a edge reinforcement system feature. |
interface |
EditBoundaryBuilder
Used to create a
EditBoundaryBuilder which
is used to change the boundaries and split knuckle locations of profile systems. |
interface |
GenericPlateSystemBuilder
This class is used to create or edit a
GenericPlateSystem feature. |
interface |
HullBuilder
This class is used to create or edit a
Hull feature. |
interface |
LongitudinalBulkheadBuilder
This class is used to create or edit a
LongitudinalBulkhead feature. |
interface |
PillarSystemBuilder
Represents a
PillarSystem builder which is used to create or edit a pillar system feature. |
interface |
PlateSystemBuilder
This class is used to create or edit the information shared between all the Basic Design plate system
features in the Ship Design application.
|
interface |
ProfileSystemBuilder
This class is used to create or edit the information shared between all the Basic Design profile system
features in the Ship Design application.
|
interface |
SeamBuilder
A
SeamBuilder used to create or edit a
ship design Seam feature. |
interface |
SmartRuleBuilder
Represents a
SmartRule builder
To create a new instance of this class, use ShipCollection.createSmartRuleBuilder(nxopen.features.shipdesign.SmartRule) Created in NX8.0.0 |
interface |
StiffenerSystemBuilder
This class is used to create or edit a
StiffenerSystem feature. |
interface |
SubSystemBuilder
This class is used to
edit the Sub System Definition of a
SubSystems feature. |
interface |
SubSystemsBuilder
This class is used to
edit a
SubSystems feature. |
interface |
TransverseBulkheadBuilder
This class is used to create or edit a
TransverseBulkhead feature. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.