public interface GenericPlateSystemBuilder extends PlateSystemBuilder
GenericPlateSystem
feature.
ShipCollection.createGenericPlateSystemBuilder(nxopen.features.shipdesign.GenericPlateSystem)
Property | Value |
---|---|
Offset.Value | 0 (millimeters part), 0 (inches part) |
Primary | FwdPortToInUp |
PrimaryOnReference | FwdPortToInUp |
Secondary1 | FwdPortToInUp |
Secondary1OnReference | FwdPortToInUp |
Secondary2 | FwdPortToInUp |
Secondary2OnReference | FwdPortToInUp |
Modifier and Type | Interface and Description |
---|---|
static class |
GenericPlateSystemBuilder.Types
Indicates the method that is being used to define the mold face of the generic plate system.
|
PlateSystemBuilder.StiffenerDirectionType
FeatureParmsBuilder.OrientationAngleRuleTypes
Modifier and Type | Method and Description |
---|---|
PlaneListBuilderList |
moldFacePlaneList()
Returns the list of planes defined to define the mold face.
|
SelectDatumPlaneList |
moldFacePlanes()
Returns the planes selected to define the mold face.
|
SelectBody |
moldFaceSheet()
Returns the sheet body selected to define the mold face.
|
void |
setType(GenericPlateSystemBuilder.Types type)
License requirements: nx_ship_basic ("Ship Basic Design") . |
GenericPlateSystemBuilder.Types |
type()
Returns the method used to define the mold face of the generic plate system.
|
boundaryPlane, boundarySection, boundarySheets, cleanUpTemporaryCurves, createRegionBody, deletePreviewBody, deleteRegionBody, offset, primary, primaryOnReference, projectionDirection, regions, secondary1, secondary1OnReference, secondary2, secondary2OnReference, setBoundaryPlane, setKnuckleEdges, setPreviewOption, setPrimary, setPrimaryOnReference, setRegionIndex, setRegionPoints, setSecondary1, setSecondary1OnReference, setSecondary2, setSecondary2OnReference, setSplitEdgeUpdateFlag, setTightness, shipNames, splitKnuckleEdges, stock, thicknessDirection, tightness, weld
angleTolerance, createPlaneForList, distanceTolerance, orientationAngleRule, setAngleTolerance, setDistanceTolerance, setOrientationAngleRule
commitFeature, getFeature, hideInternalParentFeatureAfterEdit, parentFeatureInternal, patchSolutionFlag, patchSurfaceFilename, setParentFeatureInternal, setParentFeatureInternal, setPatchSolutionFlag, setPatchSurfaceFilename, setSurroundingPatchSurfaceFilename, showInternalParentFeatureForEdit, surroundingPatchSurfaceFilename, unsetParentFeatureInternal
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
SelectBody moldFaceSheet() throws NXException, RemoteException
GenericPlateSystemBuilder.Types.SHEET_BODY
.
NXException
RemoteException
SelectDatumPlaneList moldFacePlanes() throws NXException, RemoteException
GenericPlateSystemBuilder.Types.PLANES
.
NXException
RemoteException
PlaneListBuilderList moldFacePlaneList() throws NXException, RemoteException
GenericPlateSystemBuilder.Types.PLANES
.
NXException
RemoteException
GenericPlateSystemBuilder.Types type() throws NXException, RemoteException
NXException
RemoteException
void setType(GenericPlateSystemBuilder.Types type) throws NXException, RemoteException
type
- NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.