Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static FeatureParmsBuilder.OrientationAngleRuleTypes |
FeatureParmsBuilder.OrientationAngleRuleTypes.RIGHT_HAND
Angles are measured based on a right hand rule.
|
static FeatureParmsBuilder.OrientationAngleRuleTypes |
FeatureParmsBuilder.OrientationAngleRuleTypes.SHIP_ORIENTATION
Angles are measured based on location and orientation in the ship.
|
Modifier and Type | Method and Description |
---|---|
FeatureParmsBuilder.OrientationAngleRuleTypes |
StiffenerBuilder.orientationAngleRule()
Returns the angle rule to use when measuring angles.
|
FeatureParmsBuilder.OrientationAngleRuleTypes |
FeatureParmsBuilder.orientationAngleRule()
Returns the angle rule to use when measuring angles.
|
static FeatureParmsBuilder.OrientationAngleRuleTypes |
FeatureParmsBuilder.OrientationAngleRuleTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FeatureParmsBuilder.OrientationAngleRuleTypes |
FeatureParmsBuilder.OrientationAngleRuleTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FeatureParmsBuilder.OrientationAngleRuleTypes[] |
FeatureParmsBuilder.OrientationAngleRuleTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StiffenerBuilder.setOrientationAngleRule(FeatureParmsBuilder.OrientationAngleRuleTypes angleRule)
License requirements: nx_ship_detail ("Ship Detail Design") . |
void |
FeatureParmsBuilder.setOrientationAngleRule(FeatureParmsBuilder.OrientationAngleRuleTypes angleRule)
License requirements: nx_ship_concept ("Ship Concept") OR nx_ship_basic ("Ship Basic Design") OR nx_ship_detail ("Ship Detail Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.