public static class FeatureParmsBuilder.OrientationAngleRuleTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_RIGHT_HAND
Angles are measured based on a right hand rule.
|
static int |
_SHIP_ORIENTATION
Angles are measured based on location and orientation in the ship.
|
static FeatureParmsBuilder.OrientationAngleRuleTypes |
RIGHT_HAND
Angles are measured based on a right hand rule.
|
static FeatureParmsBuilder.OrientationAngleRuleTypes |
SHIP_ORIENTATION
Angles are measured based on location and orientation in the ship.
|
Modifier and Type | Method and Description |
---|---|
static FeatureParmsBuilder.OrientationAngleRuleTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FeatureParmsBuilder.OrientationAngleRuleTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FeatureParmsBuilder.OrientationAngleRuleTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final FeatureParmsBuilder.OrientationAngleRuleTypes RIGHT_HAND
public static final FeatureParmsBuilder.OrientationAngleRuleTypes SHIP_ORIENTATION
public static final int _RIGHT_HAND
public static final int _SHIP_ORIENTATION
public static FeatureParmsBuilder.OrientationAngleRuleTypes valueOf(int value)
public static FeatureParmsBuilder.OrientationAngleRuleTypes valueOf(String name)
public static FeatureParmsBuilder.OrientationAngleRuleTypes[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.