Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Method and Description |
---|---|
CornerCutListItemBuilder |
ShipCollection.createCornerCutListitemBuilder()
Creates a
CornerCutListItemBuilder
License requirements: nx_ship_detail ("Ship Detail Design") Created in NX8.5.0 |
Modifier and Type | Method and Description |
---|---|
CornerCutListItemBuilder |
CornerCutListItemBuilderList.findItem(int index)
Returns the object at the input index.
|
CornerCutListItemBuilder[] |
CornerCutListItemBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
CornerCutListItemBuilderList.append(CornerCutListItemBuilder object)
Appends an object to the list
License requirements: None. |
void |
CornerCutListItemBuilderList.append(CornerCutListItemBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
CornerCutListItemBuilderList.erase(CornerCutListItemBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
CornerCutListItemBuilderList.erase(CornerCutListItemBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
CornerCutListItemBuilderList.findIndex(CornerCutListItemBuilder obj)
Finds the index where the input object appears.
|
void |
CornerCutListItemBuilderList.insert(int location,
CornerCutListItemBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
CornerCutListItemBuilderList.setContents(CornerCutListItemBuilder[] objects)
Sets the contents of the entire list.
|
void |
CornerCutListItemBuilderList.swap(CornerCutListItemBuilder object1,
CornerCutListItemBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.