Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static CopyPasteNewBuilder.CopyApproach |
CopyPasteNewBuilder.CopyApproach.COPY_SOURCE_FEATURES_AND_REPARENT
The approach by copy source features and reparenting.
|
static CopyPasteNewBuilder.CopyApproach |
CopyPasteNewBuilder.CopyApproach.TRANSFERRING_LINKED_BODY
The approach by transferring linked body.
|
Modifier and Type | Method and Description |
---|---|
CopyPasteNewBuilder.CopyApproach |
CopyPasteNewBuilder.copyApproachOption()
Returns an option to determine the approach to copy the ship standard parts between planes.
|
static CopyPasteNewBuilder.CopyApproach |
CopyPasteNewBuilder.CopyApproach.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CopyPasteNewBuilder.CopyApproach |
CopyPasteNewBuilder.CopyApproach.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CopyPasteNewBuilder.CopyApproach[] |
CopyPasteNewBuilder.CopyApproach.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CopyPasteNewBuilder.setCopyApproachOption(CopyPasteNewBuilder.CopyApproach copyApproachOption)
License requirements: nx_ship_detail ("Ship Detail Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.