public static class CopyPasteNewBuilder.CopyApproach extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_COPY_SOURCE_FEATURES_AND_REPARENT
The approach by copy source features and reparenting.
|
static int |
_TRANSFERRING_LINKED_BODY
The approach by transferring linked body.
|
static CopyPasteNewBuilder.CopyApproach |
COPY_SOURCE_FEATURES_AND_REPARENT
The approach by copy source features and reparenting.
|
static CopyPasteNewBuilder.CopyApproach |
TRANSFERRING_LINKED_BODY
The approach by transferring linked body.
|
Modifier and Type | Method and Description |
---|---|
static CopyPasteNewBuilder.CopyApproach |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CopyPasteNewBuilder.CopyApproach |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CopyPasteNewBuilder.CopyApproach[] |
values()
Returns an array that contains the values for this enum.
|
public static final CopyPasteNewBuilder.CopyApproach TRANSFERRING_LINKED_BODY
public static final CopyPasteNewBuilder.CopyApproach COPY_SOURCE_FEATURES_AND_REPARENT
public static final int _TRANSFERRING_LINKED_BODY
public static final int _COPY_SOURCE_FEATURES_AND_REPARENT
public static CopyPasteNewBuilder.CopyApproach valueOf(int value)
public static CopyPasteNewBuilder.CopyApproach valueOf(String name)
public static CopyPasteNewBuilder.CopyApproach[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.