Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static VirtualCurveBuilder.Types |
VirtualCurveBuilder.Types.BLEND_CENTERLINE
Blend centerline
|
static VirtualCurveBuilder.Types |
VirtualCurveBuilder.Types.ROTATION_AXIS
Rotation axis
|
static VirtualCurveBuilder.Types |
VirtualCurveBuilder.Types.VIRTUAL_INTERSECTION
Virtual intersection
|
Modifier and Type | Method and Description |
---|---|
VirtualCurveBuilder.Types |
VirtualCurveBuilder.type()
Returns the type
License requirements: None. |
static VirtualCurveBuilder.Types |
VirtualCurveBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static VirtualCurveBuilder.Types |
VirtualCurveBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static VirtualCurveBuilder.Types[] |
VirtualCurveBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
VirtualCurveBuilder.setType(VirtualCurveBuilder.Types type)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.