Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static VariableOffsetBuilder.MethodOptions |
VariableOffsetBuilder.MethodOptions.CUBIC
cublic offset applied along both of U and V directions
|
static VariableOffsetBuilder.MethodOptions |
VariableOffsetBuilder.MethodOptions.LINEAR
linear offset applied along both of U and V directions
|
Modifier and Type | Method and Description |
---|---|
VariableOffsetBuilder.MethodOptions |
VariableOffsetBuilder.method()
Returns the offset method
License requirements: None. |
static VariableOffsetBuilder.MethodOptions |
VariableOffsetBuilder.MethodOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static VariableOffsetBuilder.MethodOptions |
VariableOffsetBuilder.MethodOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static VariableOffsetBuilder.MethodOptions[] |
VariableOffsetBuilder.MethodOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
VariableOffsetBuilder.setMethod(VariableOffsetBuilder.MethodOptions method)
License requirements: studio_free_form ("STUDIO FREE FORM") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.