Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static VarOffsetFaceBuilder.Continuity |
VarOffsetFaceBuilder.Continuity.CONNECTED |
static VarOffsetFaceBuilder.Continuity |
VarOffsetFaceBuilder.Continuity.TANGENT |
Modifier and Type | Method and Description |
---|---|
VarOffsetFaceBuilder.Continuity |
VarOffsetFaceBuilder.bridgeContinuity()
Returns the bridge continuity
License requirements: None. |
static VarOffsetFaceBuilder.Continuity |
VarOffsetFaceBuilder.Continuity.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static VarOffsetFaceBuilder.Continuity |
VarOffsetFaceBuilder.Continuity.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static VarOffsetFaceBuilder.Continuity[] |
VarOffsetFaceBuilder.Continuity.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
VarOffsetFaceBuilder.setBridgeContinuity(VarOffsetFaceBuilder.Continuity bridgeContinuity)
License requirements: studio_free_form ("STUDIO FREE FORM") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.