Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static TrimExtendBuilder.ExtensionMethods |
TrimExtendBuilder.ExtensionMethods.MIRRORED
Mirrored
|
static TrimExtendBuilder.ExtensionMethods |
TrimExtendBuilder.ExtensionMethods.NATURAL_CURVATURE
Natural Curvature
|
static TrimExtendBuilder.ExtensionMethods |
TrimExtendBuilder.ExtensionMethods.NATURAL_TANGENT
Natural Tangent
|
Modifier and Type | Method and Description |
---|---|
TrimExtendBuilder.ExtensionMethods |
TrimExtendBuilder.extensionMethod()
Returns the trim extend extension method to specify the continuity of an extend operation
License requirements: None. |
static TrimExtendBuilder.ExtensionMethods |
TrimExtendBuilder.ExtensionMethods.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TrimExtendBuilder.ExtensionMethods |
TrimExtendBuilder.ExtensionMethods.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TrimExtendBuilder.ExtensionMethods[] |
TrimExtendBuilder.ExtensionMethods.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TrimExtendBuilder.setExtensionMethod(TrimExtendBuilder.ExtensionMethods extensionMethod)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.