Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static TrimCurveBuilder.InteresectionDirectionOptions |
TrimCurveBuilder.InteresectionDirectionOptions.ALONG_AVECTOR
Along a vector
|
static TrimCurveBuilder.InteresectionDirectionOptions |
TrimCurveBuilder.InteresectionDirectionOptions.ALONG_SCREEN_NORMAL
Along screen normal
|
static TrimCurveBuilder.InteresectionDirectionOptions |
TrimCurveBuilder.InteresectionDirectionOptions.RELATIVE_TO_WCS
Relative to WCS
|
static TrimCurveBuilder.InteresectionDirectionOptions |
TrimCurveBuilder.InteresectionDirectionOptions.SHORTEST3D_DISTANCE
Shortest 3d distance
|
Modifier and Type | Method and Description |
---|---|
TrimCurveBuilder.InteresectionDirectionOptions |
TrimCurveBuilder.interesectionDirectionOption()
Returns the method the system uses to find object intersections
License requirements: None. |
static TrimCurveBuilder.InteresectionDirectionOptions |
TrimCurveBuilder.InteresectionDirectionOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TrimCurveBuilder.InteresectionDirectionOptions |
TrimCurveBuilder.InteresectionDirectionOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TrimCurveBuilder.InteresectionDirectionOptions[] |
TrimCurveBuilder.InteresectionDirectionOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TrimCurveBuilder.setInteresectionDirectionOption(TrimCurveBuilder.InteresectionDirectionOptions interesectionDirectionOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.