Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static TrimCurveBuilder.CurveExtensionTypes |
TrimCurveBuilder.CurveExtensionTypes.CIRCULAR
Circular
|
static TrimCurveBuilder.CurveExtensionTypes |
TrimCurveBuilder.CurveExtensionTypes.LINEAR
Linear
|
static TrimCurveBuilder.CurveExtensionTypes |
TrimCurveBuilder.CurveExtensionTypes.NATURAL
Natural
|
static TrimCurveBuilder.CurveExtensionTypes |
TrimCurveBuilder.CurveExtensionTypes.NONE
None
|
Modifier and Type | Method and Description |
---|---|
TrimCurveBuilder.CurveExtensionTypes |
TrimCurveBuilder.curveExtensionType()
Returns the shape of the extension, if the curve to be trimmed is to be extended
to its bounding object(s)
License requirements: None. |
static TrimCurveBuilder.CurveExtensionTypes |
TrimCurveBuilder.CurveExtensionTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TrimCurveBuilder.CurveExtensionTypes |
TrimCurveBuilder.CurveExtensionTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TrimCurveBuilder.CurveExtensionTypes[] |
TrimCurveBuilder.CurveExtensionTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TrimCurveBuilder.setCurveExtensionType(TrimCurveBuilder.CurveExtensionTypes curveExtensionType)
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.