Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static TrimCurveBuilder.CurveEndOptions |
TrimCurveBuilder.CurveEndOptions.END
Trim curve from end
|
static TrimCurveBuilder.CurveEndOptions |
TrimCurveBuilder.CurveEndOptions.START
Trim curve from start
|
Modifier and Type | Method and Description |
---|---|
TrimCurveBuilder.CurveEndOptions |
TrimCurveBuilder.curveEndOption()
Returns the end of the curve that would be trimmed
License requirements: None. |
static TrimCurveBuilder.CurveEndOptions |
TrimCurveBuilder.CurveEndOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TrimCurveBuilder.CurveEndOptions |
TrimCurveBuilder.CurveEndOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TrimCurveBuilder.CurveEndOptions[] |
TrimCurveBuilder.CurveEndOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TrimCurveBuilder.setCurveEndOption(TrimCurveBuilder.CurveEndOptions curveEndOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.