Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static ToolingBoxBuilder.Types |
ToolingBoxBuilder.Types.BOUNDED_BLOCK
bounded block
|
static ToolingBoxBuilder.Types |
ToolingBoxBuilder.Types.BOUNDED_CYLINDER
bounded cylinder
|
static ToolingBoxBuilder.Types |
ToolingBoxBuilder.Types.CENTER_AND_LENGTHS
block with center point and lengths
|
Modifier and Type | Method and Description |
---|---|
ToolingBoxBuilder.Types |
ToolingBoxBuilder.type()
Returns the box type.
|
static ToolingBoxBuilder.Types |
ToolingBoxBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ToolingBoxBuilder.Types |
ToolingBoxBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ToolingBoxBuilder.Types[] |
ToolingBoxBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ToolingBoxBuilder.setType(ToolingBoxBuilder.Types type)
License requirements: ug_mold_design ("UG MOLD") OR nx_electrode_wizard ("NX Electrode Wizard") OR prog_die_wizard ("UG/Progressive Die Wizard") OR studio_free_form ("STUDIO FREE FORM") OR features_modeling ("FEATURES MODELING") OR solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.