Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static ThroughCurvesBuilder.PatchTypes |
ThroughCurvesBuilder.PatchTypes.MATCH_STRING
patch match string.
|
static ThroughCurvesBuilder.PatchTypes |
ThroughCurvesBuilder.PatchTypes.MULTIPLE
multiple patches.
|
static ThroughCurvesBuilder.PatchTypes |
ThroughCurvesBuilder.PatchTypes.SINGLE
single patch.
|
Modifier and Type | Method and Description |
---|---|
ThroughCurvesBuilder.PatchTypes |
ThroughCurvesBuilder.patchType()
Returns the patch type.
|
static ThroughCurvesBuilder.PatchTypes |
ThroughCurvesBuilder.PatchTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ThroughCurvesBuilder.PatchTypes |
ThroughCurvesBuilder.PatchTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ThroughCurvesBuilder.PatchTypes[] |
ThroughCurvesBuilder.PatchTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ThroughCurvesBuilder.setPatchType(ThroughCurvesBuilder.PatchTypes patchType)
License requirements: features_modeling ("FEATURES MODELING") OR nx_freeform_1 ("basic freeform modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.