Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static ThroughCurvesBuilder.ConstructionMethod |
ThroughCurvesBuilder.ConstructionMethod.NORMAL
Use the standard procedures.
|
static ThroughCurvesBuilder.ConstructionMethod |
ThroughCurvesBuilder.ConstructionMethod.SIMPLE
Build the simplest mesh surface possible.
|
static ThroughCurvesBuilder.ConstructionMethod |
ThroughCurvesBuilder.ConstructionMethod.SPLINE_POINTS
Use the points and tangent values at the points for reparameterizing curves.
|
Modifier and Type | Method and Description |
---|---|
ThroughCurvesBuilder.ConstructionMethod |
ThroughCurvesBuilder.construction()
Returns the construction options.
|
static ThroughCurvesBuilder.ConstructionMethod |
ThroughCurvesBuilder.ConstructionMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ThroughCurvesBuilder.ConstructionMethod |
ThroughCurvesBuilder.ConstructionMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ThroughCurvesBuilder.ConstructionMethod[] |
ThroughCurvesBuilder.ConstructionMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ThroughCurvesBuilder.setConstruction(ThroughCurvesBuilder.ConstructionMethod construction)
License requirements: features_modeling ("FEATURES MODELING") OR nx_freeform_1 ("basic freeform modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.