Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static TextBuilder.OnFacePlacementMethodOptions |
TextBuilder.OnFacePlacementMethodOptions.CURVES_ON_FACES
Placement on curves or edges on the faces
|
static TextBuilder.OnFacePlacementMethodOptions |
TextBuilder.OnFacePlacementMethodOptions.SECTION_PLANE
Placement on intersection curve created by a plane and the faces
|
Modifier and Type | Method and Description |
---|---|
TextBuilder.OnFacePlacementMethodOptions |
TextBuilder.onFacePlacementMethod()
Returns the placement method for
TextBuilder.Types.ON_FACE type
License requirements: None. |
static TextBuilder.OnFacePlacementMethodOptions |
TextBuilder.OnFacePlacementMethodOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TextBuilder.OnFacePlacementMethodOptions |
TextBuilder.OnFacePlacementMethodOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TextBuilder.OnFacePlacementMethodOptions[] |
TextBuilder.OnFacePlacementMethodOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TextBuilder.setOnFacePlacementMethod(TextBuilder.OnFacePlacementMethodOptions placementMethod)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.