Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static SweptVolumeBuilder.SweepOrient |
SweptVolumeBuilder.SweepOrient.NORMAL_TO_PATH
Normal to Path
|
static SweptVolumeBuilder.SweepOrient |
SweptVolumeBuilder.SweepOrient.PARALLEL_TO_BODY
ParallelToBody
|
Modifier and Type | Method and Description |
---|---|
SweptVolumeBuilder.SweepOrient |
SweptVolumeBuilder.sweepOrientation()
Returns the sweep orientation
License requirements: None. |
static SweptVolumeBuilder.SweepOrient |
SweptVolumeBuilder.SweepOrient.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SweptVolumeBuilder.SweepOrient |
SweptVolumeBuilder.SweepOrient.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SweptVolumeBuilder.SweepOrient[] |
SweptVolumeBuilder.SweepOrient.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SweptVolumeBuilder.setSweepOrientation(SweptVolumeBuilder.SweepOrient sweepOrientation)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.