Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static SweptBuilder.SectionLocationTypes |
SweptBuilder.SectionLocationTypes.ANYWHERE_ALONG_GUIDES
Anywhere along Guides
|
static SweptBuilder.SectionLocationTypes |
SweptBuilder.SectionLocationTypes.ENDS_OF_GUIDES
Ends of Guides
|
Modifier and Type | Method and Description |
---|---|
SweptBuilder.SectionLocationTypes |
SweptBuilder.sectionLocation()
Returns the section location option.
|
static SweptBuilder.SectionLocationTypes |
SweptBuilder.SectionLocationTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SweptBuilder.SectionLocationTypes |
SweptBuilder.SectionLocationTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SweptBuilder.SectionLocationTypes[] |
SweptBuilder.SectionLocationTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SweptBuilder.setSectionLocation(SweptBuilder.SectionLocationTypes sectionLocation)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.