Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static StyledCornerBuilder.InteriorCurveTypes |
StyledCornerBuilder.InteriorCurveTypes.ISO_CURVE_U
Iso u type
|
static StyledCornerBuilder.InteriorCurveTypes |
StyledCornerBuilder.InteriorCurveTypes.ISO_CURVE_UV
Iso u and iso v type
|
static StyledCornerBuilder.InteriorCurveTypes |
StyledCornerBuilder.InteriorCurveTypes.ISO_CURVE_V
Iso v type
|
static StyledCornerBuilder.InteriorCurveTypes |
StyledCornerBuilder.InteriorCurveTypes.NONE
No interior curve
|
Modifier and Type | Method and Description |
---|---|
StyledCornerBuilder.InteriorCurveTypes |
StyledCornerBuilder.interiorCurveType()
Returns the interior curve type
License requirements: None. |
static StyledCornerBuilder.InteriorCurveTypes |
StyledCornerBuilder.InteriorCurveTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StyledCornerBuilder.InteriorCurveTypes |
StyledCornerBuilder.InteriorCurveTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StyledCornerBuilder.InteriorCurveTypes[] |
StyledCornerBuilder.InteriorCurveTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StyledCornerBuilder.setInteriorCurveType(StyledCornerBuilder.InteriorCurveTypes interiorCurveType)
License requirements: studio_free_form ("STUDIO FREE FORM") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.