Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static StudioXformBuilderEx.SurfaceDirectionType |
StudioXformBuilderEx.SurfaceDirectionType.U
U direction of a B-Surface
|
static StudioXformBuilderEx.SurfaceDirectionType |
StudioXformBuilderEx.SurfaceDirectionType.V
V direction of a B-Surface
|
Modifier and Type | Method and Description |
---|---|
static StudioXformBuilderEx.SurfaceDirectionType |
StudioXformBuilderEx.SurfaceDirectionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StudioXformBuilderEx.SurfaceDirectionType |
StudioXformBuilderEx.SurfaceDirectionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StudioXformBuilderEx.SurfaceDirectionType[] |
StudioXformBuilderEx.SurfaceDirectionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StudioXformBuilderEx.insertPole(NXObject xformObject,
int poleIndex,
StudioXformBuilderEx.InsertPoleType insertType,
StudioXformBuilderEx.SurfaceDirectionType direction,
double location)
Inserts a pole in the selected xform object
License requirements: studio_free_form ("STUDIO FREE FORM") . |
void |
StudioXformBuilderEx.removePole(NXObject xformObject,
int poleIndex,
StudioXformBuilderEx.SurfaceDirectionType direction)
Inserts a pole in the selected xform object
License requirements: studio_free_form ("STUDIO FREE FORM") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.