Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static StudioXformBuilderEx.PoleEditType |
StudioXformBuilderEx.PoleEditType.CONSTRAINED
Edited maintaining constraint
|
static StudioXformBuilderEx.PoleEditType |
StudioXformBuilderEx.PoleEditType.FREE
Edited without maintaining constraint
|
static StudioXformBuilderEx.PoleEditType |
StudioXformBuilderEx.PoleEditType.NONE
Not edited
|
Modifier and Type | Method and Description |
---|---|
static StudioXformBuilderEx.PoleEditType |
StudioXformBuilderEx.PoleEditType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StudioXformBuilderEx.PoleEditType |
StudioXformBuilderEx.PoleEditType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StudioXformBuilderEx.PoleEditType[] |
StudioXformBuilderEx.PoleEditType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StudioXformBuilderEx.setPoleEditType(NXObject xformObject,
int index,
StudioXformBuilderEx.PoleEditType poleEditType)
Update pole status of the selected BSpine curve
License requirements: studio_free_form ("STUDIO FREE FORM") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.