Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static StudioXformBuilderEx.AdvancedMethodType |
StudioXformBuilderEx.AdvancedMethodType.ADVANCE_OFF
Deprecated.
Turn off advanced methods
|
static StudioXformBuilderEx.AdvancedMethodType |
StudioXformBuilderEx.AdvancedMethodType.FALLOFF
Deprecated.
Fall off, it is deprecated in NX85 release
|
static StudioXformBuilderEx.AdvancedMethodType |
StudioXformBuilderEx.AdvancedMethodType.INSERT_KNOT
Deprecated.
Insert knot
|
static StudioXformBuilderEx.AdvancedMethodType |
StudioXformBuilderEx.AdvancedMethodType.KEEP_CONTINUITY
Deprecated.
Keep continuity, it is deprecated in NX85 release
|
static StudioXformBuilderEx.AdvancedMethodType |
StudioXformBuilderEx.AdvancedMethodType.LOCK_REGION
Deprecated.
Lock region
|
static StudioXformBuilderEx.AdvancedMethodType |
StudioXformBuilderEx.AdvancedMethodType.PROPORTIONAL_MOVEMENT
Deprecated.
Proportional movement
|
Modifier and Type | Method and Description |
---|---|
StudioXformBuilderEx.AdvancedMethodType |
StudioXformBuilderEx.advancedMethod()
Deprecated.
Deprecated in NX8.5.0. Use
StudioXformBuilderEx.advancedMethodOption() instead.
|
static StudioXformBuilderEx.AdvancedMethodType |
StudioXformBuilderEx.AdvancedMethodType.valueOf(int value)
Deprecated.
Returns the enum constant of the specified enum type with the specified value.
|
static StudioXformBuilderEx.AdvancedMethodType |
StudioXformBuilderEx.AdvancedMethodType.valueOf(String name)
Deprecated.
Returns the enum constant of the specified enum type with the specified name.
|
static StudioXformBuilderEx.AdvancedMethodType[] |
StudioXformBuilderEx.AdvancedMethodType.values()
Deprecated.
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StudioXformBuilderEx.setAdvancedMethod(StudioXformBuilderEx.AdvancedMethodType advancedMethod)
Deprecated.
Deprecated in NX8.5.0. Use
StudioXformBuilderEx.setAdvancedMethodOption(nxopen.features.StudioXformBuilderEx.AdvancedMethodOptionType) instead.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.