Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static StudioXformBuilder.Types |
StudioXformBuilder.Types.PLANARIZE_ROW_OF_POLES
Planarize type of Xform
|
static StudioXformBuilder.Types |
StudioXformBuilder.Types.ROTATE
Rotate type of Xform
|
static StudioXformBuilder.Types |
StudioXformBuilder.Types.SCALE
Scale type of Xform
|
static StudioXformBuilder.Types |
StudioXformBuilder.Types.TRANLSATE_ALONG_CONTROL_POLYGON
Along polygon type of Xform
|
static StudioXformBuilder.Types |
StudioXformBuilder.Types.TRANSLATE
Translate type of Xform
|
static StudioXformBuilder.Types |
StudioXformBuilder.Types.TRANSLATE_NORMAL_TO_FACE_OR_CURVE
Along normal type of Xform
|
Modifier and Type | Method and Description |
---|---|
StudioXformBuilder.Types |
StudioXformBuilder.type()
Deprecated.
Deprecated in NX8.5.0. Use
StudioXformBuilderEx instead.
|
static StudioXformBuilder.Types |
StudioXformBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StudioXformBuilder.Types |
StudioXformBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StudioXformBuilder.Types[] |
StudioXformBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StudioXformBuilder.setType(StudioXformBuilder.Types type)
Deprecated.
Deprecated in NX8.5.0. Use
StudioXformBuilderEx instead.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.